(0)| 9/26/2008 7:44 AM | |
|
Joined: 3/28/2008 Last visit: 11/13/2025 Posts: 38 Rating:
|
HI every body I am facing two problems with WinCC. Problem1: I am using User archive for storing my data. Also i am using user archive table to view the data in WinCC runtime. I am using control tags for retrieving and saving values in user archive tables. In user archive table when i am rwriting tags, error showing "Error while executing the Write tags functions". Screen dump attached. Also i checked the user achive editor. it tells there is no error in User archive configuration. Screen dump attached. SCADA - WinCC V6.2 SP2 Problem2: I am not able to open SQL Enterprise Manager. its shows an error "Connection failed, check SQL Server Registration properties". Screen dumps attached. its happened in WinCC V6.0 SP4, SQL Server 200 Is this problem faced by anybody else. Can any one guide me to solve this issue.? Regards Shiv AttachmentWinCC Errors.zip (101 Downloads) |
Follow us on