(0)| 2/9/2020 8:15 AM | |
|
Posts: 7 Rating:
|
Hi! During commissioning of a 802d sl pro somewhere in the process, I think when the connection with Starter or PCL program went wrong this alarm 8022 appeared. Does anyone know how to solve this? It is possible to JOG the axis but the alarm is active all the time. Full alarm message: 008022 Option 'activation of more than 5324KB SRAM' not set The message is also described in the manual but this is above my expertise to understand at the moment. My only solution now would be to redo the commissioning. Diagnostic manual: https://cache.industry.siemens.com/dl/files/651/28823651/att_65265/v1/802Dsl_DIA_0607_en.pdf Thanks! |
Last edited by: geahr at: 02/09/2020 08:52:37 |
|
Follow us on