(0)| 2/9/2020 8:26 AM | |
|
Posts: 1250 Rating:
|
How about this. |
| 2/11/2020 2:58 PM | |
|
Joined: 3/2/2007 Last visit: 1/20/2026 Posts: 1004 Rating:
|
If we supply the 3RV2922-1CP0 from after the breaker, then it will detect the off by hand? |
|
... thank you ... |
|
| 2/12/2020 7:27 AM | |
|
Joined: 3/2/2007 Last visit: 1/20/2026 Posts: 1004 Rating:
|
Is the 3VA9988-0AA21 suitable to be mounted on these breakers? 3VA1032-4ED32-0AA0 , circuit breaker 3VA1 IEC frame 100 breaking capacity class S Icu=36kA @ 415V 3-pole, line protection TM210, FTFM, In=32A overload protection Ir=32A fixed short-circuit protection Ii=10 x In nut keeper kit 3VA1040-4ED32-0AA0 , circuit breaker 3VA1 IEC frame 100 breaking capacity class S Icu=36kA @ 415V 3-pole, line protection TM210, FTFM, In=40A overload protection Ir=40A fixed short-circuit protection Ii=10 x In nut keeper kit 3VA9988-0AA21 , LEADING CHANGEOVER SWITCH CHANGEOVER CONTACTS TYPE HP (14MM) ACCESSORY FOR 3VA1 and 3VA20 up to 3VA25 (can this one be mounted on the above two breakers?) |
|
... thank you ... |
|
| 2/13/2020 3:58 PM | |
|
Joined: 3/2/2007 Last visit: 1/20/2026 Posts: 1004 Rating:
|
So, this is a good combination? 3VA1132-4ED32-0AA0 , circuit breaker 3VA1 IEC frame 160 breaking capacity class S Icu=36kA @ 415V 3-pole, line protection TM210, FTFM, In=32A overload protection Ir=32A fixed short-circuit protection Ii=10 x In nut keeper kit 3VA1140-4ED32-0AA0 , circuit breaker 3VA1 IEC frame 160 breaking capacity class S Icu=36kA @ 415V 3-pole, line protection TM210, FTFM, In=40A overload protection Ir=40A fixed short-circuit protection Ii=10 x In nut keeper kit 3VA9988-0AA23 , LEADING CHANGEOVER SWITCH CHANGEOVER CONTACTS TYPE HQ (7MM) ELECTRONIC ACCESSORY FOR 3VA1 and 3VA20 up to 3VA25 |
|
... thank you ... |
|
Follow us on