(0)| 2/17/2020 6:33 PM | |
|
Posts: 4 Rating:
|
Dear all, I'm working with a Sinamics G130 (CU320) connected to a P-DP network (S7-400 as master). I have three numbers sinamics drive g130 using for the same applications , i have one drive failure and replaced by new one ,I have done download all parameters from good drive to new drive , but when I want to starting the new drive from DCS drive not start , but when I go to start the drive from local AOP30 it was ok 👌 , when i check some paramters like p810 in new drive not same parameter in old drive Old drive parameters MOT 13-210 2016 ParameterParameter text"MOT13-210". 1 p3 BOP access level [4] Service [3] Expert 2 p918 PROFIBUS address 45 47 3 p21000[0] Run-time group properties, Run-time group 1 [1] T = 1 * r21002, Free run-time group _1 4 p21601 Profibus_Active Control_Unit : r2043.2 5 p21602 Remote_CMD_Active Drive_1 : r2093.0 6 p21603 HW_Switch_local Control_Unit : r723.4 7 p21604 Spare_Cmd_Sel 1 8 p21701 Start_Push_button Control_Unit : r722.0 9 p21702 Start_Input2 0 10 p21703 Start_Input3 0 Does not exist 11 p21704 Start_Input4 0 12 p21801 Running Drive_1 : r899.1 13 p21802 Fault_Reset_Loc Control_Unit : r722.2 14 p21805 Flt_Reset_NoRun Control_Unit : r21804.0 15 p21806 CDS_Change Drive_1 : r50.0 16 p21807 Stop_PushButton_Local Control_Unit : r723.1 17 p21808 Stop_Spare 0 18 p21901 Start_Cmd Control_Unit : r21705.0 19 p21902 Stop_Cmd Control_Unit : r21809.0 20 p22001 CDS_Status Drive_1 : r50.0 New drive parameters Control_UnitDrive_unit_1.Control_UnitUnit All above parameters showings Dose not exist ------------------------------------------------------------------------------------------ |
Last edited by: Algeelani at: 02/17/2020 21:21:20Last edited by: Jen_Moderator at: 02/18/2020 06:09:25New subject after splitting |
|
| 2/17/2020 9:48 PM | |
|
Posts: 4 Rating:
|
Ok, noticed with thanks |
Follow us on