3/3/2020 9:59 AM | |
Joined: 1/27/2020 Last visit: 9/27/2021 Posts: 14 Rating:
|
Hello, I have a problem with the PN Connection .
I can't get any further with step 2.4 on "Using the Test App" by "4. Press 9 to set the PN Driver to the mode “Operate”". I don't get any feedback from the Test_App. Best regards |
Last edited by: M4RC at: 03/03/2020 10:10:18 |
|
3/3/2020 4:08 PM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello, We would have to take a deeper look at your config and TIA Portal project to see why this is not working correctly. Maybe you could compress and upload it on here? Alternatively, have you checked if this application example is working fine for you? Kind regards! |
3/3/2020 4:39 PM | |
Joined: 1/27/2020 Last visit: 9/27/2021 Posts: 14 Rating:
|
Thanks for the fast answer. I want to connect the IoT2040 and the S7-1200 SPS. The SPS has to be an I-Device, to get a Master-Slave-System with the IoT. Unfortunately I have problems generating the XML file for the IoT. As an alternative I have generated the GSDML file for the coupling with PN Driver. And i know the PLC I-Device and PN Driver should not be coupled directly in the project. There is already a topic for this, but it does not help me. https://support.industry.siemens.com/tf/ww/en/posts/profinet-s7-1200-and-iot2040/229923/?page=0&pageSize=10 In the Attachment you can see my TIA Project without the GSDML file. Greetings AttachmentIOT2040_TestProjekt.zip (262 Downloads) |
Follow us on