(0)| 10/13/2008 4:54 PM | |
|
Posts: 22 Rating:
|
no, i have installed SIMATIC NET 2005 HF1 as you can read in WinCC compatibility matrix. it is strange: i have read in st7cc pdf manual (page 18) about Simatic net 2006 but at page 31 of the same manual you can read : "Step 8: Select the products you want to install. Activate the options SIMATIC NET PC Software V6.x... and SIMATIC NCM PC/S7 V5.3+SP2." Well, simatic net 2005 hf1 is the version 6.3. It is not clear the right version... AttachmentWinCC_V6_Kompatiblitaets_e.pdf (425 Downloads) |
Last edited by: rafmg at: 10/13/2008 4:57 PM |
|
| 10/23/2008 2:03 PM | |||
|
Posts: 5822 Rating:
|
Hello, I fear this is a problem I can not help... it seems to be development related. Therefore I would strongly recommend to you to contact the international Customer Support. You can do that either by using the
or you call +49(0) 180 5050 222 "€ 0.14 /min. from the German landline network, mobile telephone prices may vary" or you send a FAX to +49(0) 180 5050 223 "€ 0.14 /min. from the German landline network, mobile telephone prices may vary" I hope the people there may help you to solve this problem. Best regards J_Bell |
||
| 11/28/2008 11:11 PM | |
|
Posts: 22 Rating:
|
Simply solution: st7cc work correctly only if WinCC installation Language is German or English. |
Follow us on