(0)| 3/5/2020 3:10 PM | |
|
Posts: 1 Rating:
|
Dear All I need to compare the values of two counter values in 0BA3 logo. If two values are equal then an "1" as an output. How to do it.
|
| 3/5/2020 4:13 PM | |
|
Joined: 12/18/2014 Last visit: 1/22/2026 Posts: 36503 Rating:
|
Hello Ibrar899, at first welcome to the forum. What you want isn't possible with a LOGO! 0BA3. |
| 3/5/2020 5:17 PM | |
|
Joined: 2/22/2008 Last visit: 4/25/2025 Posts: 2698 Rating:
|
If you only need a forward counter with small values, you can create your own counters with pulse relays. Then you can compare the values, but you only have 56 blocks for the program and not much memory for retentivity. See attachment for example. Regards, Scorp AttachmentCounter 0BA3.zip (242 Downloads) |
| 3/5/2020 9:10 PM | |
|
Posts: 66 Rating:
|
Hi, Perhaps this is not possible with a 0BA3 (I still don't get all the differences between the various numbers This compares 2 counters (now activted by I1 and I2) and activates output Q1 when equal. Hope this helps Edit: I now see you don't have the mathematic instruction available on the 0BA3... sorry. AttachmentCounter Compare.zip (248 Downloads) |
Last edited by: Luna08 at: 03/05/2020 21:11:55 |
|
Follow us on