(4)| 2/10/2020 8:36 PM | |
|
Posts: 1250 Rating:
|
Have a look at this example. It is version and needs to be upgraded first to TIASP13-SP1/ or SP2 so that it can be opened in later versions. I converted it to TIA13SP2 and attached it. (Siemens was great to respond and upgraded the project to TIA 14 and 15) There are two projects; look in the FIll _bottle project and you will see how they addressed the HSC technology object directly by it's database.
You can do the same to address your counter; that's one way of doing it. To see the HSC database go to the project tree?Technology object and right click on the HSC>then from the context menu select Open DB editor In the code you will see how the new count value was reset to zero. In your case you will use this code in a start OB and set the value to the one save in the retentive tag. The file is too big to attach so I uploaded to mega where you can download it and hopefully the moderator will upload it too. I also contact Siemens to add an upgraded version as I find this example very helpful. |
Last edited by: Jen_Moderator at: 02/11/2020 09:26:35Optimized link. Last edited by: Kal.A at: 02/12/2020 17:16:51 |
|
| 2/12/2020 5:21 PM | |
|
Posts: 54 Rating:
|
Thank you Mr. Kal.A , I will try. |
| 3/7/2020 7:45 AM | |
|
Posts: 54 Rating:
|
THANK YOU MR. Kal.A , NOW IT'S OK THANKS BROTHER, YOU TEACH ME. |
This contribution was helpful to
|
|
Follow us on