(1)| 3/6/2020 9:22 AM | |
|
Joined: 1/21/2016 Last visit: 2/7/2025 Posts: 88 Rating:
|
Hello, I have a mechanic with 2 motors controlled by 2 S210. I have a translation movement to perform. The two motors are synchronized. The problem is that I can not do the tunning of only one engine at a time, the mechanics do not allow me, indeed the two axes of translation are mechanically linked (I attached a diagram to understand (Sorry I'm not very good at drawing). I would like to know if it was possible to perform an auto tuning in synchronization. Cordially. AttachmentSchéma.pdf (204 Downloads) |
|
Cordially, |
|
| 3/6/2020 11:36 AM | |
|
Joined: 4/28/2015 Last visit: 5/2/2025 Posts: 43 Rating:
|
-Removed- |
Last edited by: Axel Scholz at: 03/06/2020 17:10:18Grüße, Axel |
|
Follow us on