(2)| 1/22/2017 2:11 PM | |
|
Joined: 12/12/2008 Last visit: 5/20/2025 Posts: 69 Rating:
|
One question: In the IOT Manual, it is stated: X2, Ethernet2 ready for PoE In what way is it ready for PoE? Can I use PoE to supply power to the IoT2040, or can the IoT2040 power some remote device? Is this implemented? BR Ben ------------------------------------------------------------------------------------------ |
Last edited by: Ben1902 at: 1/22/2017 2:12:20 PMLast edited by: Min_Moderator at: 1/23/2017 12:44:14 PMNew subject after splitting |
|
| 1/23/2017 8:29 AM | |
|
Joined: 4/28/2015 Last visit: 1/15/2026 Posts: 3345 Rating:
|
Hi, the POE functionality is only prepared, so it is not a Plug&Play solution. There is an additional hardware part required that has to be soldered to the IOT. For the Galileo Gen2 there is an entry in their forum: https://communities.intel.com/thread/55354 Here is an additional link where you can see where to solder the device: http://www.intel.com/content/www/us/en/support/boards-and-kits/intel-galileo-boards/000006223.html The holes for soldering are the same, IOT and Galileo Gen2. The POE acts not as a source, it is only possible to power the IOT2000. Best regards! |
|
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to
|
|
| 3/9/2020 6:41 PM | |
|
Joined: 5/18/2019 Last visit: 8/8/2024 Posts: 1 Rating:
|
Hi,
Best regards Manlio AttachmentPhotos.zip (337 Downloads) |
Last edited by: AutoGen_404907 at: 03/09/2020 18:50:44 |
|
This contribution was helpful to
|
|
Follow us on