(0)| 3/8/2020 11:12 AM | |
|
Joined: 6/23/2008 Last visit: 1/16/2026 Posts: 1174 Rating:
|
Dear all, I should communicate to a S7-200 SMART of type 6ES7288-1SR20-0AA0. My CPU is 410-5H. I would like to use PUT and GET on my side. I have searched already and found some topics in forum and also read data sheet and the relevant chapter in the S7-200 SMART System manual. It's still not 100% clear to me if I can use PUT/GET from S7-400 side. The data sheet says (on page 4) that S7 communication as client and server is supported by this S7-200 SMART CPU. The S7-200 SMART System manual says in chapter 8 'Communication' under ethernet:"S7 peer-to-peer communication with other S7-200 SMART CPUs" I wonder know about"...with other S7-200 SMART CPUs". Does it mean that with a S7-200 SMART CPU I can only communicate with other S7-200 SMART CPU but not to an S7-300/400 in regard to S7 communication? I hope that there is a user from Asia who has expierence on this issue and can help in regard to this question. Thanks.. |
Last edited by: mark1507 at: 03/08/2020 11:13:03Last edited by: mark1507 at: 03/08/2020 11:14:01"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
Follow us on