(0)| 3/19/2020 5:32 PM | |
|
Joined: 11/7/2019 Last visit: 12/12/2025 Posts: 21 Rating:
|
Nobody? |
| 3/20/2020 3:36 PM | |
|
Joined: 11/7/2019 Last visit: 12/12/2025 Posts: 21 Rating:
|
nobody ? thank. Regard. |
| 3/20/2020 4:24 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, Please have some patience. It's not like we are online all the time. Please try to formulate your question better. I think you're confusing APL_OP_BUTTON with analog values you want to change. What do you want to do exactly? If you want to have 5 buttons (BOOL) to be pressed in one APL_OP_BUTTON, yes it's possible. Each button has it's own variable. Configure the BinLink1-5 and BinAuthorizationLevel 1-5 with your variables Set BinCount to 5 Set picture: @PG_APL_OA_Binary105.pdl for OpAreaPicture Set the correct permissions for button 1-5 You can configure a maximum of 5 buttons in a APL_OP_BUTTON. If you need more, you have to do some modifications, but it's not a simple task. Read the APL_Styleguide document to get familiair. |
Last edited by: Oreca at: 03/20/2020 18:02:21If I could help you, you can use the RATE button. Thank you. |
|
| 3/20/2020 9:48 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Such as thing is possible, but you need to make modifications to the standard object. You made a custom block right? I suggest you will try to create it APL style (see the APL Styleguide). Then you won't need a lot of modifications if you follow the rules. In the scripts, there is a piece of code (see below) which reads the bit of a DWORD (status). You can make a code with this to write the correct bit. Something to get you on the way... But preferred is to make 5 BOOL signals in your custom block, with the correct attributes like S7_m_c, Op_Level and then create it the same way like Siemens does in the APL faceplates. One hint, reset the variable at then end of your code. So the faceplate will set the bit, execute the function in the code and then resets itself at the end. That is APL style.
|
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on