(0)| 3/25/2020 7:15 PM | |
|
Posts: 1 Rating:
|
I have now experienced 2 separate drives, different sizes, that have faulted on Fan Speed. At first I though it may be due to the fan starter, but it has now occurred after the fan was running constantly for over an hour. I am reluctant to bypass the fault in case there is a problem with the fan speed. What can be causing the problem with the fan speed detection? What should I check to prevent the fan speed detection from falling? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/26/2020 10:25:23New subject after splitting |
|
Follow us on