(0)| 4/2/2020 8:16 AM | |
|
Posts: 36 Rating:
|
Hello, I have the same problem. I am very beginner with this G120 communication and etc. I use G120 CU250S-2 PN and I can go online with it start the comissioning in the comissioning panel but the motor measurement "LED" is yellow and some enables are missing. Using Tia Portal V15.1 Later I would like to control the G120 by a PLC (S7-1200). And some moments later the flashing gone and the PLC started not able to reach the drive and the PLC modules shown some errors. That's why I tried to do it from the basics again. Thank you! Lehel ------------------------------------------------------------------------------------------ Attachmentsome enables are missing.zip (180 Downloads) |
Last edited by: hajleh12 at: 04/02/2020 08:20:03Last edited by: Jen_Moderator at: 04/02/2020 09:55:57New subject after splitting |
|
Follow us on