(0)| 4/12/2020 9:57 PM | |
|
Posts: 42 Rating:
|
Hi Peterakos, Would you mind append this code that you comment? Mostly the part of changing diplay values with up and down keys. Thanks a lot! |
| 4/13/2020 8:58 PM | |
|
Posts: 51 Rating:
|
@ Berguinsson, see the attached. A simple menu structure in this case it is using the TDE function keys , but you can use others or inputs. To make clear i also used inputs 1 & 2 that can also trigger a screen to be active and the same function keys to work. this setup i have used many times in the past , the menus structure is not my idea, i do not know when or where i found it but i used it a lot Of course you need to adjust based on you requirements but on this way you can use more screens. In one project (for legal reasons can can not show it) i used 8 screens with nearly the same text only a small change and i used program steps to trigger every screen. to keep the user informend where the proccess was at that step/time. Attachmentmulti screen menu.zip (187 Downloads) |
Follow us on