(0)| 3/26/2020 5:06 PM | |
|
Joined: 2/6/2019 Last visit: 9/18/2024 Posts: 10 Rating:
|
Dear Friends. I have got the same problem, F7995 but during startup. There are 5 motors in project, all V90's and all work except one. Checked and compared all the parameters. The drive just will not home, with F7995 ("Motor indentification fault") in the screen on the drive. When i push the motor by hand it 'picks up' and starts the homeing like normal. Somebody has an idea? The P1982 parameter, suggested above, i do not have.. Motor is a 1FL6-2AF21-1AA1 (400Watt, inc, 2500, no brake) and the drive is a 6SL3210-5FB10-4UF1 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/27/2020 08:55:26New subject after splitting |
|
Follow us on