(0)| 3/24/2020 8:28 AM | |
|
Posts: 3 Rating:
|
Hi all, I am trying to print to a default printer connected by USB to a TP1200 Comfort panel. I am using the postscript V1.4 driver and want to print a print report. However when it prints the print report, I am getting a printout of the parameters for the label, then it says image followed by a lot of u and + and prints half a roll of paper. Is the print report an image or a text file? or is the printer not compatible, it is a mylox ml228-usb-v? If I connect the printer to the USB port of a laptop and print a text file it works perfectly, but not when connected to the TP1200 panel. How do I create a dummy log? where is this done? and then if I copy the created text file to it would this print as a text file or does the panel file have its on extension, thus not working on this printer. if so is it possible to load a generic text only driver into the comfort panel? Regards R1cky ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/24/2020 09:37:10New subject after splitting |
|
| 4/8/2020 2:18 PM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello which TIA Portal Version and Image Version on the Panel do you use? which printer do you use? do you use one of the released printers with the Comfort Panels? https://support.industry.siemens.com/cs/ww/en/view/11376409 Bye Murof |
Last edited by: Murof at: 04/08/2020 14:19:04If this Information really helps, you could use the Rate function |
|
Follow us on