(1)| 4/18/2020 5:43 PM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hi, Check my thread at PCS7 Complete Overview and see the links under "APL forum links" |
|
If I could help you, you can use the RATE button. Thank you. |
|
| 4/18/2020 6:14 PM | |
|
Posts: 5 Rating:
|
Hi, I already read your post (https://support.industry.siemens.com/tf/us/en/posts/custom-block-icon/151745/?page=0&pageSize=10#post612021 ) but, i wonder that Can I use this feature for own analog/motor etc. block and own wincc block icon? or This feature is just for PCS7. |
| 4/18/2020 7:42 PM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hi, Yes ofcourse you can. I recommend reading the APL styleguide in order to create blocks that fit APL standard. Like using attributes for block, using structure inputs/outputs etc. Very important. When the block is ready, you can create block icon and faceplates. I highly suggest using a existing block icon like a VlvL with it's faceplates because making your own faceplates is difficult. Rather you adjust the faceplates yourself. All can be found under the links I described. |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
Follow us on