(2)| 2/27/2017 8:55 AM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hi, If you install the correct package from the DVD like ES, OS single station, OS server, all necessary components are installed including Simatic Net and its subcomponents. Please check if this is done correctly |
|
If I could help you, you can use the RATE button. Thank you. |
|
| 3/2/2017 7:37 AM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hi moelsayed, Not exactly, The Configuration Editor is something different than Communication settings, but they are related. Communication Settings: Configuration, Commissioning and Diagnostics of the communication of a PC station. Configuration Editor: Central Management for components of the PC station like modules and applications. It can be compared by inserting a component in the rack of an CPU. You can download the configuration data from Step 7. See the print screen to located the Configuration Editor. Do you have it? |
Last edited by: Oreca at: 3/2/2017 7:38:05 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on