4/30/2020 6:24 AM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello, you can refer to requirements on third party motors for S120, which are shown here. But even without detailed data of the motor and encoder system, I would expect, that these motors can be used with SINAMICS S120 as well.
|
With best regards, |
|
This contribution was helpful to
1 thankful Users |
5/3/2020 10:56 AM | |
Joined: 4/27/2020 Last visit: 4/25/2025 Posts: 4 Rating:
|
Hello Many thanks for your reply . In attach you can find the pictures of the name plate of the servomotor and it's old model SIEMENS drive . In addition to my first question I have another question . As you can see in the pictures currently used drive produces 3PH 230 V in it's output , but as I found out just blocksize model of sinamic S120 have 3ph 220V input and output . In our factory it's better that we use book size model with one control unit , one line module and several motor modules as multi axis control ( I think it's more economical ) but book size models have only 3ph 380 V input. What is your solution for this matter ? Best regards. AttachmentPicture.zip (125 Downloads) |
5/4/2020 10:29 AM | |
Joined: 4/27/2020 Last visit: 4/25/2025 Posts: 4 Rating:
|
Hi Yes I have connected the Masterdrives infeed to a 3AC220V line . Best regards. |
5/5/2020 9:40 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating:
|
Yes see listmanual description of parameter p210. |
Follow us on