(1)| 5/7/2020 9:57 AM | |
|
Posts: 36 Rating:
|
Hello everyone! I have some questions about basic positioning is TIAPortal. in TIAP V14 SP1 I am using SINA_POS FB284 for positioning. 1. Everything looks fine until I want to rise the rpm over ~600 (Velocity=6000), the drive gives me a double error (F07452 & F07490). I would like to know how can I make it work with a higher speed. 2. I can't use Mode: 2 (relative positioning). When I choose it the EnableAxis input goes to "0" and when I switch it back to "1" the Mode goes from 2 to 3 (positioning as setup) and nothing really happening. Anything what I made wrong? AttachmentPictures_1_6.zip (355 Downloads) |
Follow us on