5/8/2020 2:38 PM | |
Joined: 3/14/2008 Last visit: 9/24/2025 Posts: 2217 Rating:
|
Hi, The inputs of the Interlock blocks (Inx) have the s7 attribute: BLK_Jump. When a block is connected to this input which has s7_m_c attributes, the jump to faceplate button is showing. It is correct that a regular AND block or timer block does not work because it has no operator attributes. When a block has s7_m_c attributes, it means those variables are compiled to the OS. In order to let this work, you have to connect a block with s7_m_c attribute. Apart from this, a faceplate must exist as well of the block that is connected. You can however use the following block that is included in the Industry Library: SelFp. This is a block that has 5 SelFP variables, all with BLK_Jump attribute. You can connect up to 5 blocks which allow jump to faceplate. Maybe you can use such functionality? See attachment. You can create your own block as well by using the attribute: BLK_Jump. |
Last edited by: Oreca at: 05/08/2020 14:41:45If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
Follow us on