5/11/2020 11:15 PM | |
Joined: 7/4/2012 Last visit: 9/8/2025 Posts: 13 Rating:
|
Hello experts! I'm having some problem in communicating S120 CU320 and S7-1500 CPU 1511 over Profinet. I have Tia V15.1 and support package S120 StartDrive I'm using SINA_POS block and still having a problem, the output "Error" is TRUE and the "Status" is 16#8601 and "DiagID" is 16#8090 The CU320-2PN "RDY" led is GREEN and "COM" led is GREEN. I know that the error is about the function "DPWRT_DAT", I already check the hardware ID, device name, and all of that seems ok. If someone could help me out, if I missing some parameter, communication related or its a logic error in the PLC. Attached the archive project TIa V15.1 Thank you in advance. AttachmentS120_SinaPos.zip (217 Downloads) |
Follow us on