(0)| 5/16/2020 5:07 PM | |
|
Posts: 42 Rating:
|
Hello ixo65. The rest of the code doesn't have relation with the screen. I only show the amplifier blocks of the screen on the display. Regards. |
| 5/16/2020 5:11 PM | |
|
Joined: 12/18/2014 Last visit: 1/21/2026 Posts: 36500 Rating:
|
You ask for help. If you don't want... |
| 5/16/2020 6:24 PM | |
|
Posts: 42 Rating:
|
Here is my code. As summary: At the top-left side i show values on the display pressing left key six times. At the top-right i read modbus values(temperature sensor values) and i compare with two values in the UDF, then i active a flag. Below this part of code is where i have the problem. i want to read the somes values(32=16 measurements resolutions+16 measurements intervals) sent from the LWE and display them on the logo screen, but i am only able to display 16 values. Thank you su much. AttachmentLogo valor float2.zip (197 Downloads) |
| 5/16/2020 6:54 PM | |
|
Joined: 2/22/2008 Last visit: 4/25/2025 Posts: 2698 Rating:
|
Maybe there is a solution, but i have not tried it out up to now. All values you only need to show in a text message can be mapped to an analog multiplexer, see example in attachment. You also must use the VM mapping for the analog multiplexer to map max. 4 words. I hope, the values from your modbus device will overwrite the values of the multiplexer, but i don't know it. I can't test it in the moment, maybe someone else have the equipment at home. Normally you can use NAI1 - NAI32 for network analog inputs. If you get problems by copying a part of the diagram, then also try to add single NAIx. Regards, Scorp AttachmentMappings.zip (206 Downloads) |
Follow us on