(4)| 5/26/2020 11:41 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, Yes, this is possible. You can just change the variables in CFC. Beware if you are using EMT or EPHT, the variables must be ignored to be able to write them in the CFC chart. Also, when an EPH controls an EM, the EM variables cannot be changed either. |
|
If I could help you, you can use the RATE button. Thank you. |
|
| 5/27/2020 1:13 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, The SFC is set to MANUAL, so the automatic commands like START/COMPLETE/ABORT etc. do not work. Put the SFC in auto by toggling AUT. Take a look at the Compendium manual for SFC's. Link .It seems you have little experience with SFC types (which is not a problem ofcourse |
Last edited by: Oreca at: 05/27/2020 13:20:18If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 5/27/2020 5:59 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Just set PARAM to "1" always and you're good |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
Follow us on