(0)| 7/8/2020 7:43 PM | |
|
Joined: 7/26/2016 Last visit: 11/6/2024 Posts: 4 Rating:
|
Hi I have a problem, please help me I have a CPU Simatic ET 200SP that I cannot start in RUN, because the error 16# 02:4042 (Description: CPU error: Hardware configuration error Incorrect Base Unit: Central bus error due to incorrect type of plugged module CPU changes to STOP mode, new startup inhibit set: - Unacceptable difference between expected and actual confiquration DQ 8X24VDC/o.5A ST_1) I check the HW, it is correct. I unload the programm from CPU and download it again to CPU, but nothing has changed. there is mechanical vibration in my installation
What can I do? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/09/2020 09:39:01New subject after splitting |
|
Follow us on