(1)| 5/2/2006 2:46 PM | |
|
Posts: 1084 Rating:
|
[quote user="Waterboy"]I guess there is some confusrion. WinCC has Zoom in\out feature but I guess it does not tell you in percentage (100 % for that matter). Within Graphic Designer open "View" -> "Toolbars" and select "Zoom". Now you have a zoom toolbar that tells you the percentage. [quote user="Waterboy"]Secondly I tried it with Line Weight = 1 and the whole screen visible i.e. 100 % zoom not more that that....still it showed up as straight line. - Which version of wincc are you using? - Is the Line Style of the line still set to dash dot after you have drawn the line? (just look at the properties). I will include a pdl file created with wincc v6.0 sp2 hf5 in which a line is drawn with the line style dash dot. with regards, Ikkezelf AttachmentDashDot.zip (668 Downloads) |
| 5/3/2006 6:28 PM | |
|
Posts: 85 Rating:
|
Great !!! That's why I like you people. Thanks a lot. |
Follow us on