(0)| 7/16/2020 5:09 PM | |
|
Joined: 5/6/2019 Last visit: 5/23/2025 Posts: 82 Rating:
|
I am trying SBT using S71500 + Sinamics S120 drive and the motor 1fk7022 5ak70. I am using communication via SIC/SCC - telegram 701 for the brake test. I followed the Safety Integrated Function Manual. As per session 5.8.4 for configuring the telegram 701 . I selected p0922 = p2079 = telegram 5 . Therefore p2070 and p2071 = 9 p60122 = telegram 701 For programming the TIA I used Fail safe library LDrvSafe . My configuration of the drive and the results are seen in the attached document. When I run the test stop I am getting the corresponding bits in the status word . But when I run the brake test, I am not seeing "brake test selected" from the status word (S_ZSW3B) . The other status word - fr eg S_ZSW1B are updated. Procedure of testing I am giving rising edge to the enable of the control and the status block to activate LDrvSafe block. I am giving "LDrvSafe_SinaTlg701Control_DB".selectBrakeTest and "LDrvSafe_SinaTlg701Control_DB".startBrakeTest = TRUE PS.As per my understanding now, this is the topic heading. I can change the heading when I find the real cause of the problem. AttachmentSBT_Tel701.pdf (334 Downloads) |
| 7/17/2020 4:23 PM | |
|
Joined: 5/6/2019 Last visit: 5/23/2025 Posts: 82 Rating:
|
Hello, Thank you for the help. I did teststop to check if that is working. yes, I removed teststop and then I got this Brake Control Error (10). The SBC is enabled and motor holding brake is selected as configuration. I have followed the requirements and enabling criteria for SBT from the manual. Could that be a programming error? AttachmentSBT_Tel701_v2.pdf (351 Downloads) |
| 7/20/2020 1:42 PM | |
|
Joined: 5/6/2019 Last visit: 5/23/2025 Posts: 82 Rating:
|
Also my p1278 = 0 ( brake control with diagnositc evaluation ) and SBC enabled My power module is PM 240-2 |
| 7/23/2020 11:39 AM | |
|
Joined: 10/11/2006 Last visit: 1/21/2026 Posts: 6052 Rating:
|
Hello,
|
|
With best regards, |
|
Follow us on