7/27/2020 2:36 PM | |
Joined: 9/3/2014 Last visit: 2/13/2025 Posts: 79 Rating:
|
Dear Friend, Thanks a lot for your response. Attached you can see two electrical drawings, the first one is a KEB frequency inverter drive with capacitors, the second one is a Control Techniques. We were replacing the frequency inverters when any is damaged and I have installed a Siemens one, but I have had problems when there is a energy cut off because the machine has a not wanted behavior. So the only thing that I need to do is to connect the capacitors bank, but I am not sure if I can do it with Siemens G120. Finally, Could you please, make a lillte drawing about your design? I don't want to do anything wrong. Thanks in advance. Best regards.
AttachmentInverters.pdf (316 Downloads) |
Follow us on