(0)| 7/31/2020 2:04 AM | |
|
Posts: 14 Rating:
|
I have one weighing project to finish but I need help from you guys to finish this project. I am new to PLC and HMI Programming. Given below link shows the password-protected program and HMI screen with functions key on it. I can not see what is going inside the program right now and I want to make a change inside the PLC program. As you can see the 2nd link that there is HMI screen but Infield I don't have HMI with me, all I want is to control different things using push buttons or selector switch instead of HMI. I want to use the physical button to switch on the service mode first and then one more selector switch to add maximum weight value (let's say I want to add 14 then I move my selector switch to left and If I want to add 15 then move it to right) and then lastly it will save the value inside the program using another push button. How do I modify this HMI screen button with an actual physical button? so that I don't have to use HMI anymore in field. Thanks in Advance. [snip] AttachmentScreenshots.zip (298 Downloads) |
Last edited by: Jen_Moderator at: 07/31/2020 06:54:26Removed links and added files as an attachment. |
|
| 7/31/2020 10:33 AM | |
|
Joined: 1/4/2007 Last visit: 1/13/2026 Posts: 1198 Rating:
|
Hello dearj06, Well, I recommend you to take a look to the following video on YouTube: In this video, the communication is explained from: In this video, the WP251 is explained. But this video is also valid for the WP231 module:
Best regards Siwarexi |
Last edited by: Jen_Moderator at: 07/31/2020 11:21:52Embedded video. |
|
This contribution was helpful to
|
|
| 7/31/2020 2:41 PM | |
|
Posts: 14 Rating:
|
Thank you for the reply, I managed to solve problem <3 |
Follow us on