(0)| 8/10/2020 2:57 PM | |
|
Posts: 6 Rating:
|
Hi mark1507, I have same doubt about it. what i used is S7-410E Redundancy and ET200SP HA redundant I/Os for a package level system, understood that diagnostic can be generated in operator station automatically, but what i would like to know is how to read diagnostic in user program, eg. wire broken, short circuit, over/under flow, master/slave of I/O channel, so can send the status to other system like DCS, which FB to be used for DI/DO/AI/AO? is it channel basis or module basis? Appreciated if sample project provided, thank you very much! Best Regards ------------------------------------------------------------------------------------------ |
Last edited by: buddy1222 at: 08/10/2020 15:12:15Last edited by: Jen_Moderator at: 08/11/2020 08:32:57New subject after splitting |
|
Follow us on