(0)| 8/13/2020 1:01 PM | |
|
Posts: 7 Rating:
|
Dear All, Considering the fact that AFS is discontinued and there won't be a "Coupler Redundancy" option available anymore, still sometimes, like in my case due to existing cabling, we may need a "redundant interface + single trunk cable" solution. So I'm wondering if Ring Topology is accepted, then why two chained FF Couplers cant be accepted. To explain the proposed topology I've drawn a diagram which is attached. T-Junction in my sketch can be a regular H1 junction box. Please keep in mind that I'm not saying it works. I'm asking whether it works or not and if not, then why?! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/13/2020 13:53:03New subject after splitting |
|
Follow us on