(0)| 1/6/2009 8:25 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello spm_cpl, Look at this decisions: How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher? You can give us more details about systems and what you want to do... regards |
| 1/7/2009 1:58 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello spm_cpl, Well, let's start one by one: 1. You buy new PC with simple ethernet card. 2. You need to order SimaticNet with license, but version tha support win98. 3. Build connection PC (simple ehernet card to CP1430). 4. Now you must connect OPC Server (PC) with Wonderware Intouch. Use OPCLink to connect Intouch with OPC Simatic Net Server. How look there: Configuring OPCLink Using TCP/IP and a Standard Network Card for Windows NT 4.0 to Access S7-400 PLCs via the Siemens S7 OPC Server 5. You don't needPCES5 card(hardware), PCLINK(software), and H1Server... regards |
| 1/9/2009 3:21 PM | |
|
Posts: 25 Rating:
|
Thank you, UMENCHO. I will try to do, if I still have problem about this, I'll post later. Thanks All. |
| 1/10/2009 8:34 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello spm_cpl, You are wellcome! regards |
Follow us on