(0)| 9/2/2020 3:38 PM | |
|
Posts: 5 Rating:
|
replace a CPU 417-4h to a CPU 410-5H, once the hadware was compiled and downloaded, I proceeded to download the user program (OBs, FBs, FCs), it threw me the following message:"unable to copy the block". And it happens that I cannot download the program to the CPU, I was inquiring through siemens support, I found the following: “The download you are trying to download is a STEP 7 mechanism that is blocked for the CPU 410-5h that only downloads with PCS7 (CFC) (therefore it works for CPU 417-4H and not for CPU 410). " If this is the case, how can I download the user program (ob, fc, fb) should there be a procedure to download the program or some hotfix that allows downloading in step 7 in this type of CPU 410-5H. Regards RSG ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/03/2020 06:26:26New subject after splitting |
|
| 9/2/2020 3:49 PM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi, The CPU410 can only be used in conjunction with PCS7.
|
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on