(1)| 9/1/2020 7:22 PM | |
|
Joined: 10/25/2017 Last visit: 9/4/2025 Posts: 5 Rating:
|
Hey guys Trying to get KP900 keys as bits and control leds. According to this entry i configured basic network with CPU 1211C and KP900. Checked IO device setting in HMI properties, set transfer area to I100...103 and Q100...103. HMI and PLC are well connected and basic access with tags working except for keys. When i press any button on panel all bits I100.x - I103.7 in plc are stay zero. Same with leds: if i activate for example in PLC Q100.0 no one led is light. Can someone explain how to do it right? Solved. Check "Profinet IO enabled" in the HMI windows settings (before project startup). |
Last edited by: Jen_Moderator at: 09/02/2020 08:14:55Optimized link. Last edited by: AutoGen_4513916 at: 09/05/2020 17:39:46 |
|
| 9/2/2020 9:36 AM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Hi, What version of TIA portal do you use? Best regards Wizard |
| 9/2/2020 9:39 AM | |
|
Joined: 10/25/2017 Last visit: 9/4/2025 Posts: 5 Rating:
|
15.1 |
Follow us on