(0)| 9/8/2020 1:02 PM | |
|
Posts: 9 Rating:
|
Hi, I hope all are doing well in this difficult times. I'm also having a problem right now trying to connect to OP7 & OP17. I want to save the program using ProSave v15 in my Simatic Field PG M6 but I cannot establish a communication by using RS232 Interface, 15/9-pin, 6XV1440-2K___. I tried to connect the 15-pin male connector to IF 1A of OP7 and IF 2 of OP17 then the 9-pin female to RS232/TTY port of my PG using serial port adaptors D9/D25 but communication didn't establish. Kindly advise. Best regards, Parica ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/08/2020 14:33:09New subject after splitting |
|
Follow us on