(1)| 9/17/2020 4:23 PM | |
|
Posts: 20 Rating:
|
Hello everyone I am attempting to configure at KTP400 Basic panel. when I attempt to download to the HMI I get the following errors: download failed due to missing panel: image components with a different version are installed on the target device. I have looked at this link and it appears to have the files installed, I have also attached a screenshot of the folders. I am not sure what "DVD 3" the link below is referring to because in the kit I ordered it did not come with a DVD 3, one has 2 dvds labeled 1/2 & 2/2(6ES7822-0AA06-0YA5). But the pic of that error is the one I am getting, can`t add another attachment https://support.industry.siemens.com/cs/ww/en/view/109781234 Software Product code: 6ES7822-0AA06-0YA5 HMI part number: 6AV2 123-2DB030AX0 Thanks in advance. |
Last edited by: Controls_Tech at: 09/17/2020 16:41:47 |
|
| 9/17/2020 5:02 PM | |
|
Joined: 4/24/2006 Last visit: 1/20/2026 Posts: 9106 Rating:
|
Hello, Have a look at the following link: Image downloads for HMI operator panels Best regards, Wizard |
This contribution was helpful to
|
|
Follow us on