5/24/2017 1:50 PM | |
Posts: 6 Rating:
|
I have mv420 and tried to trigger the picture. First I sent positive singal for executing reset_MV command. After I sent positive signal busy status was on for 60 seconds. After that 60 seconds I got the error e7fe0800. I looked in manual what that mean ( Timeout during "INIT" (60 seconds according to "TC3WG9"). In tia project everything is green and i can not see any mistake. On web page of camera settings are correct. IP mode is ident prof. and connections under intgration tab are PROFINET IO. Also If I try to execute read_MV command after 60 seconds I get error e7fe0100 ( In this status, only the "Reset_Reader" command ("WRITE-CONFIG") is permitted ). I guess if I solve first mistake with reset command the second one will be automaticly solved. In attachment you have some screenshots from my simualtion. Does anyone know how can i solve e7fe0800 error? What did I do wrong ? Thank you. Attachmentmv420.zip (925 Downloads) |
5/24/2017 3:32 PM | |
Posts: 6 Rating:
|
Hi Owei, I tried also that but alse doesnt help. I made somewhere mistake and I can not see the mistake. :( |
3/20/2019 12:40 PM | |
Joined: 1/15/2019 Last visit: 2/23/2023 Posts: 1 Rating:
|
Hi rumba, Could you solve your problem? I have the same problem.. |
9/29/2020 2:59 PM | |
Joined: 1/3/2013 Last visit: 9/5/2025 Posts: 42 Rating:
|
Dear friends, I was struggling with same errors. Then I decided to take an test all HW & SW combinations My MV440 UR has the V07.00.02_06 firmware. First scenario, I used the MV440 UR GSDML file that comes with this Applications Example. In TIA Portal HW configuration I used the Ident Profile v7.0 that comes with the associated GSDML file. I tried both MvControl FB provided in the example and individual functions to Reset, Change Program and Read MV....in both cases the results were errors like: E7FE_0100, E6FE_0300 ( Program selection not possible), E6FE_0500 (reset command is required). Second scenario, I found that searching the TIA Hardware Catalogue for MV440 has found the 6GF3440-***** entry. I loaded this new HW element, and changed the Operating Mode of the 6GF3440-***** to Ident Profile since default is to use some FB. I had to reassigned the Technological Object configuration option to match my new entry in TIA HW and everything sorted out. Both the MvControl FB worked and also the individual functionalities. Other useful resources that I found: https://support.industry.siemens.com/cs/ww/en/view/103528928 https://support.industry.siemens.com/cs/ww/de/view/109757269 Best regards! |
Last edited by: Jen_Moderator at: 09/30/2020 09:23:34Optimized links. |
|
This contribution was helpful to
1 thankful Users |
Follow us on