(1)| 9/29/2020 11:59 AM | |
|
Posts: 1 Rating:
|
When I am trying to download the timer value from 300ms to 150ms in S71214, I am receiving an error as Error downloading to the device, & in message, it is showing there is not enough memory space on the CPU for this amount of data., So I checked load memory is 95% full. So what to do further, I want to do some online changes in the machine & it is a production machine. Please suggest ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/30/2020 07:58:29New subject after splitting |
|
Follow us on