(0)| 9/30/2020 5:47 PM | |
|
Joined: 2/10/2015 Last visit: 10/8/2025 Posts: 291 Rating:
|
Hello everyone, I have a wincc flexible 2008 project that I want to migrate with tai v13 sp1 but, when I start the migration with tia portal, I perceive the faults 1 and 2. When I resume again I perceive the fault 1 and 3. the original wincc project was edited with an earlier version and I have wincc flexible 2008 sp5, I opened the project with wincc and with the option "copy project step7" I made the copy but when I start the migration fault 1 and 3 still appear. I need your help to solve this problem because the console of a production line is out of service and I have another console with which I want to replace the one that is out service.see attached.thank you for helping me. receive my best regards.
Attachmentfault.zip (376 Downloads) |
| 10/5/2020 10:15 AM | |
|
Joined: 8/3/2009 Last visit: 1/21/2026 Posts: 16653 Rating:
|
Hello Franck Herve Perhaps this FAQ can help: https://support.industry.siemens.com/cs/de/en/view/109486003 You can also try to di the Migration of the WinCC flexible Project in two steps with the Migration Tool: https://support.industry.siemens.com/cs/de/en/view/58638200 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on