9/15/2020 4:01 PM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35946 Rating:
|
Start a Support Request. |
10/9/2020 10:52 AM | |
Joined: 9/19/2018 Last visit: 12/6/2024 Posts: 399 Rating:
|
I just tested the last version of the file (Opera de presa). As I can only change I1..I6 I changed the inputs to I1..I4 in SF012. It works in my LOGO!8 V1.82.02. Text and status of I1..I4 is displayed correctly. Hint: For testing I changed EN of SF012 to high. In this way I don’t need to understand the rest of the program as the Message text is displayed all the time. AttachmentOpera di presa1234.zip (246 Downloads) |
Follow us on