11/10/2020 7:50 AM | |
Posts: 11 Rating:
|
Hi , how are you . topic : 3 electric heater controlled by on off thermostats. i have logo8 with the following program needed. Manual mode :when the thermostat is on , heater can bee switched on locally using selector switch until temp reaches the set point from the thermostat then heater switch off. AUTO MODE: when thermostat is on the first heater will switch on automatically by logo ,and after 30 sec second heater will switch on and same sequence for the remaining electrical water heaters. when thermostat is off all electrical heaters will switch off. all electrical heaters must be set to auto mode using selector switch in order to enable full auto mode to all heaters. also we want to give signals to bms like auto mode selected , trip signal if any heater is trip and run status if any heater is running. thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/10/2020 12:07:28New subject after splitting |
|
11/10/2020 8:57 AM | |
Posts: 11 Rating:
|
Hi , I thought its the same topic thats why. yes i only wanna heat. best regards |
Last edited by: NAIF_221 at: 11/10/2020 09:01:51 |
|
11/10/2020 12:08 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject heater is published within the conference LOGO! - Projects. Best regards,Jen_Moderator |
Follow us on