(0)| 12/2/2020 8:15 AM | |
|
Joined: 10/11/2006 Last visit: 1/19/2026 Posts: 6069 Rating:
|
Hello, with Technologyobject it is possible to configure a load gear in the mechanic view. Page 27: Stepper motors Drives with a stepper motor interface are connected using telegram 3 and with the help of PTO (Pulse Train Output) pulse generators. For functional support of stepper motor operation, quantization of the control deviation can be set. 3.8 Mechanics (S7-1500, S7-1500T) <TO>.LoadGear.Numerator <TO>.LoadGear.Denominator https://support.industry.siemens.com/cs/ww/en/view/109766462 |
|
With best regards, |
|
Follow us on