12/2/2020 11:22 AM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Dynamic representations are a very important part of HMI / SCADA System. There are many elegant ways to show dynamic status, like Dynamic Widget, Text List, Graphic List, etc. Sometimes however what we need is just change an object color dynamically. It could be done using its “BackColor” property, for example. It is possible to control the “BackColor” property linking it with a tag, using the system function “SetPropertyValue” or by Scripting. This Simple sample shows how to do it in these three ways. Tip: The Application example FAQ “SIMATIC WinCC Unified - Tips and Tricks for Scripting (JavaScript)“ (https://support.industry.siemens.com/cs/br/en/view/109758536), chapter 5.4.5 describes how to mount color by RGB or aRGB components. Project (archived and ziped) AttachmentColors.zip (1766 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
5 thankful Users |
Follow us on