(0)| 12/9/2020 5:12 AM | |
|
Posts: 3 Rating:
|
Hello Sir, Can you please help me to solve the encoder fault F31117 in CU250S2-PN, G120 drive. I am using Simotics M-1PH1 motor which has TTL encoder. Wiring is correct as per color code. I have connected encoder to D-Sub interface. Please suggest to rectify this problem. Thanks, Ram.
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/09/2020 15:47:30New subject after splitting |
|
| 12/9/2020 5:13 PM | |
|
Joined: 7/7/2010 Last visit: 1/7/2026 Posts: 16354 Rating:
|
Are you 100% sure the encoder signal is A & A- (like +5 & -5V), B & B-, and Z & Z-? Have you put an oscilloscope on the encoder signal wires to verify they are both above and below 0V reference for each channel and that A & B channels are able to indicate direction, and that the Z channel fires only once per revolution?
|
|
science guy |
|
This contribution was helpful to
|
|
Follow us on