1/6/2009 6:46 PM | |
Posts: 1 Rating:
|
Can anyone help me! I am trying to allow a series of LED lights to turn on up the stairs with a 3 second delay on each on. I have been able to do this with 4 lots of outputs each with 4 lights on it. This will be activated by a PIR sensor at the bottom of the staircase. Once you reach the top of the staircase there is another PIR sensor that i want to turn the lights off after a minute delay. Also, i want to be able to do this in reverse coming down the staircase. Lights come on by the top sensor but then go off by the bottom PIR sensor after a minute. Can anyone help with getting this sequence with the PIR sensors. I have attached what I have done so far. The sequence runs in order when the PIR is activated at the bottom and counts down. Once the lights turn off the PIR up the top activates but I want the lights to go the opposite way. Cannot see how to do it! Attachmentstep controller.zip (701 Downloads) |
Last edited by: Mike1985 at: 1/7/2009 5:28 PM |
|
1/29/2009 12:07 PM | |
Posts: 20 Rating:
|
Hi Mike, Here is sample from entrance to top. Light is off when time is out or top PIR is activated. If do not need second function - top PIR, remove this input from program. From top to exit - the same program dublicated. Starting on I5 etc, just miror. Good luck Attachmentstep_controller.zip (688 Downloads) |
Follow us on