(3)| 12/21/2020 10:50 AM | |
|
Joined: 9/30/2016 Last visit: 1/12/2026 Posts: 953 Rating:
|
Please also see the attached screenshots. I need to add an AC drive (SINAMICS G120 CONTROL UNIT CU250S-2 PN) to my TIA project. I have the TIA portal installed on two PG's and on one of them I have the option of drives under "Add a device" but on the other (which is my main PG) drives is not an option. Why am I missing the option of adding drives on my main PG and how do I get this option? AttachmentED1 programmering c.zip (609 Downloads) |
| 12/21/2020 10:53 AM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Hello, Have you installed Startdrive? Best regards, Wizard |
| 12/21/2020 11:01 AM | |
|
Joined: 7/9/2015 Last visit: 1/15/2026 Posts: 4496 Rating:
|
Hi, you have TIA V15.1. What kind of Drives you get if you click on Drives (at you Add Device screenshot). In SINAMICS Startdrive V15 or higher SINAMICS G120, G120C, G120D, G120P und G110M as well as SINAMICS drives based on the CU310-2 or the CU320-2 are supported. Check PDF in this FAQ: Which hardware and functions of SINAMICS G130, G150, S120, S150 and SINAMICS MV are supported by SINAMICS Startdrive V15, V15.1 and V16?Regards, Towome |
|
|
|
| 12/21/2020 11:36 AM | |
|
Joined: 7/9/2015 Last visit: 1/15/2026 Posts: 4496 Rating:
|
Hi, the newest Startdrive V15.1 you get there: SINAMICS Startdrive V15.1Regards, Towome |
|
|
|
Follow us on