1/26/2009 6:50 PM | |
Joined: 10/18/2006 Last visit: 7/29/2024 Posts: 163 Rating:
|
Hi folks! I´m attaching you a project already done in PCS7 v7.0 SP2. Is there any HW incompatibility between this HW and this version of PCS7? Specially in what refers to the CP 443-1EX20... In an installation on-site we could compile and download this HW Config to the S7-400H but we couldn´t start the controller.. Only after downloading the project with Step7, the CPU started. So then, we downloaded it and tried to start it with PCS7 once again, and this second time, it worked ?!?! Any idea? Thanks a lot in advance Attachmentcomunes.zip (192 Downloads) |
1/30/2009 12:12 AM | |
Posts: 2661 Rating:
|
Hi bocatadeatun, Please look at the following FAQ: Information about manuals on the topic of "CPU and STEP 7 compatibility" |
Follow us on