1/28/2009 5:27 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello Look at PLCSim with PCS7 7.0s p1 There PLCSIM v5.3 works with PCS7 v7.0 SP1. regards |
1/28/2009 5:40 PM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi cosmetric, i think your plcsom version is right http://support.automation.siemens.com/WW/view/en/28879540 i'm sure problem is in a different position, check your application for exact error Regards |
1/28/2009 7:27 PM | |
Posts: 2661 Rating:
|
Hi cosmetric, Have you tried installing PLCSIM V5.4 SP2? Service Pack 2 for S7-PLCSIM V5.4 Regards |
1/29/2009 9:03 PM | |
Posts: 2661 Rating:
|
Hi cosmetric, There seems to be some confusion regarding the compatibility of CEMAT V6.1 SP3 and PCS7 V7.0 SP1. See the following links: Release of CEMAT V6.1 Service Pack 3 for SIMATIC PCS 7 V7.0 Update CEMAT V6.1 Service Pack 3 No where it is mentioned that CEMAT V6.1 SP3 is compatible with PCS7 V7.0 SP1. The first link states that this CEMAT version is released for PCS7 V7.0. The second link says the main requirement for CEMAT V6.1 SP3 is PCS7 V6.1 SP1. I think you should contact Siemens (details in first link above)to clarify the situation. Regards |
Follow us on