(2)| 8/21/2013 5:38 PM | |
|
Joined: 1/27/2009 Last visit: 12/10/2025 Posts: 42 Rating:
|
hi, I have PC Adapter USB V1.3 firmware 1.2.0, i want update the firmware to V1.3.1 but always got error "The target device is not responding" All LED's on PC Adapter are lit, when i click Excute button, USB Led blink for a while then the error message appear. Please advise. Regards, Ciwa
AttachmentPC Adapter.zip (1542 Downloads) |
| 8/28/2013 10:40 AM | |
|
Posts: 376 Rating:
|
hello ciwa79, could you already solve the problem? Please let us know. If not are you sure that the PC Adapter USB has not a defect? Can you still out successfullya communication between PC and S7-PLC (MPI/PROFIBUS) realizing? Here finds you more information about the SIMATIC S7, PC Adapter USB (6ES7 972-0CB20-0XA0). http://support.automation.siemens.com/WW/view/en/14692974 My recommendation for you is. If you can the problem not solved, pleaseask at the technical support for SIMATIC. Perhaps these know the problem and have a solution for you. The contact data finds you here. http://support.automation.siemens.com/WW/view/en/16605032 If you have a solution, please write short information in the forum. I am interested. Many thanks. Best regards Azteke0110 |
| 8/29/2013 8:46 AM | |
|
Joined: 1/27/2009 Last visit: 12/10/2025 Posts: 42 Rating:
|
Hello Azteke, The problem still exist, i cannot upgrade the firmware. I can communicate with S7 PLC (MPI/PROFIBUS) but in Windows XP with PC Adapter V2.0 driver only, the built-in driver in Step7 V5.5 not work for my PC Adapter. So i want to upgrade the firmware perhaps with the new firmware i can use the built-in driver in Step7 V5.5 Any advise?? Regards, Ciwa
|
| 8/30/2013 11:13 AM | |
|
Posts: 376 Rating:
|
Hello ciwa79, many thanks for the sent information. I have investigated again. But I do not know the reason for the problem. You should certainly ask at the Siemens Technical Support. There must be a solution. The contact data finds you here. Good luck! http://support.automation.siemens.com/WW/view/en/16605032 If you have a solution, please write ashort information in the forum. I am very interested. Many thanks. Best regards Azteke0110 |
| 4/15/2016 1:23 PM | |
|
Posts: 2 Rating:
|
Hello CIWA , I have the same problem as you , have you solved it yet ? Best regards Per |
| 2/5/2020 9:19 AM | |
|
Posts: 1 Rating:
|
Hi. I have exactly the same problem. is there any solution. thnx |
| 1/15/2021 3:58 PM | |
|
Joined: 10/13/2020 Last visit: 5/14/2024 Posts: 1 Rating:
|
me too, same problem did not find the solution |
Follow us on